It seems from the description in the User Guide that the CC1125 could wait listening indefinitely - is that true ?
ie, it would be up to the host microcontroller to implement a timeout ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PM said:it meets ETSI LBT spec
indeed - the ETSI spec is equally opaque on this.
PM said:you can control time out from host MCU
I know I can - the question was whether I must - ie, whether that's the only way!
EDIT
The algorithm seems to be:
START | | Start timer, Tf = 5ms | +<------------+ | | V | LISTEN | til | timer | expires | | | Start timer, | | 0 < Tps < 5ms V | channel | free? --NO-->--+ | YES | | v TRANSMIT
Which clearly has a potential endless loop.