Other Parts Discussed in Thread: CC1310, SIMPLELINK-CC13X2-26X2-SDK, SYSCONFIG, SIMPLELINK-CC13X0-SDK
Tool/software: Code Composer Studio
CCS version: Version: 9.3.0.00012
Collector = 1352P-2 Launchpad
Sensor - CC1310 Launchpad
In the Sensor and Collector - TI 15.4 Stack Project Zero, there is a part of the project that the engineer is asked to change the settings on the collector. Actual text:
"Update the reporting interval that the collector will request from the sensor: In the collector project, in config.h, set CONFIG_REPORTING_INTERVAL to 1000 (instead of 90000)"
The Sensor code has a config.h file but the Collector does not. And in doing a CNTL-H for a whole project search for "CONFIG_REPORTING_INTERVAL ", the search only turns up the Sensor's config.h file and some post-compiler files on the Collector.
So where do I adjust that parameter on the Collector code?