Hello exxperts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello exxperts,
Please see https://www.ti.com/lit/ds/symlink/cc1120.pdf: The blocking in the alternate channel for 1.2 kbps is given as 54 dB. Also see which outline some of the best blocking that is possible to achieve.
Hello TER-san,
I gave you the selectivity numbers which is different than the ACP numbers.
But when I measure ACP, it's normally in dBm or dBc. Is it specified how to measure it in the standard or if it's dBc or something else?
Hello TER-san,
Hello TER-san,
Hi,
I don't think we have these numbers in the datasheet so I would need to do some measurements. Which data rate and deviation is this?
I'm not sure if I fully understand the spec. In the first post you wrote " need to secure 70dB at 25kHz away" but then you wrote "Also, required ACP value is -56dB." Is 70 dB at the edge?
Do you have a figure that shows how this should be measured and the limits? ST T-108 has some good figures on the ACP limits, does STD-42 have the same?