Hi team,
Question from a customer-
The CC11xx users guide (SWRU295E) makes the statement “OOK modulation simply turns the PA on or off to modulate ones and zeros respectively” (Sec 5.2.2). This suggests that we should be able to generate OOK by turning the PA on and off. However….
Later, in the configuration register descriptions (PA_CFG0 – Power Amplifier Configuration Reg. 0) it makes the statement “For OOK with maximum depth the PA_POWER_RAMP-4.ASK_DEPTH must always be all zero hence for ASK/OOK with maximum depth the maximum ASK/OOK output power is 12.5dBm”
We would like to be able to generate full depth OOK (PA ‘on’ = 1 / PA ‘off’ = 0) at maximum RF output power. The first statement suggests that the hardware can do this. However the second statement suggests that this is not possible. Is there a way to generate full depth OOK at maximum RF output power? If it helps, we do not need to do pulse shaping for this application.
Thanks!
Lauren