Our project is based off LAUNCHXL-CC1310.
1. When both collector and sensor are flashed, the sensor is able to join the network and sends data on it's poll interval.
2. After the sensor sends it's data, we erase and re-flash the same sensor binary
3. We can see the PA an PC, and 6 attempts to rejoin the network, but all were unsuccessful and sensor data is never sent or received by the collector. ( We ran multiple test on different boards and the rejoin is unsuccessful 80% of the time.
Note:
If we perform #1 and ONLY cycle power on the sensor, the sensor rejoins every time.
We recompile the code with `#define CONFIG_SECURE false` and performed the same test. It rejoins and sends data every time.