Other Parts Discussed in Thread: CC2500, CC2640
i want to measure packet round-trip time using the most precise timer available on the cc1310 -- which i believe is the 24MHz general-purpose timer...
i have already configured RAT_GPO0 (packet transmit state) and RAT_GPO1 (packet receive state) to reflect their values on two GPIOs -- which i can easily measure with my logic analyzer....
but i'd really like to have the cc1310 use the GPT to do this measurement....
is it possible to set up the GPT to: 1) start counting when RAT_GPO0 goes low; and then 2) stop counting when RAT_GPO1 goes high???
thanks....