Hi,
Is it normal that when Im switching between CCS 8 and Smart RF Flash Programmer (and vice versa), I need to do some debugger update?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it normal that when Im switching between CCS 8 and Smart RF Flash Programmer (and vice versa), I need to do some debugger update?
Best regards,
Sometimes I am able to see other error:
"Error connecting to the target:
(Error -242 @ 0x0)
A router subpath could not be accessed.
The board configuration file is probably incorrect.
(Emulation package 9.3.0.00032)
"
I am trying also CCS 10.2.0.00009, it does not help.
Artur
Please make sure to use the CCS version recommended for the SDK version you are using. If you are using the latest CC1310 SDK (4.10), you should use:
Also, are you only having problems when switching between the flash programmer and CCS? Why do you need the flash programmer? Are you using the latest version?
BR
Siri