Other Parts Discussed in Thread: CC3235SF, CC3235MODSF, TMDSEMU110-U, CC3235S, CC3235MODS
Hello,
we had the CC3235SF-LaunchPad and was able to develop the application framework (based on http server example).
things worked fine. however, we noticed that there is LAUNCHCC3235MOD (CC3235MOD part) that could potentially save us time on layout/cap tuning, etc.
before buying the LAUNCHCC3235MOD to try out, can you please confirm with me the following things:
1- It seems LAUNCHCC3235MOD used MSP430 to emulate XDS110 while CC3235SF-LaunchPad use TIVA MCU to emulate the XDS110. can you please confirm from user point of view, this is all transparent? another word, i only need to hook up the USB and i can flash in the CC3235 directly from CCS (v10) flash option just like i did for the CC3235SF-LaunchPad.
2- the http server application that we have now running on CC3235SF-LaunchPad will run on LAUNCHCC3235MOD without any modification? i think this is the case because it is the same CC3235, but i just want to make sure that is the case.
I already order XDS110 box for custom board but i will try to use XDS110 box on the launch pad to see how it perform vs the built in XDS110 on launch pad.
Thanks and Best Regards,
Henry