This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220MODA: Can CC3220MODA replace CC3235MODA from a FW standpoint?

Part Number: CC3220MODA
Other Parts Discussed in Thread: CC3235MODASF

Hi team,

My customer is wanting to know if the CC3220MODASF will work in place of their CC3235MODASF. We know it will work fine from a hardware standpoint, their concern is potentially managing two separate firmware builds for the two different processors. 

Boiled down- their question is:

Can the same build output from a CC3235-based CCS 10/11 project function correctly on a CC3220 device? 

Assume two boards, one with a CC3235MODASF and the other with a CC3220MODASF.

  1. Will the same SLI file work to program both boards in manufacturing?
  2. Will the same TAR file upgrade both boards over-the-air?
  3. Is it possible for application software to tell the two boards apart during runtime using some sort of SL API call or hardware register inspection?

Thank you!
Lauren