This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a custom board with the CC3230SF and I want to program the device with Uniflash.
I installed the newest version of Uniflash 8.3.0 on my laptop, which runs a fresh installed Windows 11.
After starting Uniflash, I select under New Configuration the CC3235SF(BOOTLOADER).
Then I select the COM Port of the XDS110 and select the image from a folder.
When I click on 'Load Image", I get an error message after few seconds:
I checked the path, and the file MSPSLBootloader.dll is in the folder.
I also reinstalled Uniflash, which doesn't help.
How can I fix this problem?
Best regards
Thomas
You are not using Uniflash correctly.
CC32xx only works with Uniflash through "Image Creator".
Please refer to https://www.ti.com/lit/swru469.
When I use the "Image Creator" it works.
In the past, I used on a different laptop Uniflash 8.0 with the option CC3235SF(BOOTLOADER) and it works without any problem.
This error only appears in the new version of Uniflash 8.3.
When should I use the option CC3235SF(BOOTLOADER) and when should I use the "Image Creator"?