Part Number: CC3230SF
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi,
My customer is now trying to program the External SPI Flash on their own board with CC3230SF by using UniFlash, but they can’t program. Could you answer some their questions below ?
They’re following UniFlash ImageCreator Basics in the SimpleLink Academy for CC32xx – 7.10.00.13 in the Resource Explorer.
- Sense-On-Power (SOP) jumpers are set to 010 on their board as well.
- For using UniFlash, Both JTAG and UART are needed to connect with CC3230SF device ? Or any one interface is OK ? They’re using XDS110.
- Since My device cannot be detected automatically, they chose CC31XX / CC32XX manually.
Which device configuration should they choose from the below list in the case of their own board with CC3230SF ?

- On the above GUI screen, What do Serial and On-Chip mean ? On-Chip means on-chip Flash ?
- In the below case, only UART is connected ? Is JTAG not used ?

- For Adding the MCU Image in below, which MCU image mcuimg.bin, mcuflashimg.bin or other should they choose ? They’re using CC3230SF.
- Is it different from the case of programming the on-chip Flash or the case of external SPI Flash ?
- Is it possible to use UniFlash to program both the on-chip Flash or external SPI Flash ?
Thanks and regards,
Hideaki