Other Parts Discussed in Thread: CC3220S, CC3235SF, CC3100
Hi, I am trying to configure wifi module from TM4C1294NPCT controller
for that i am working with SDK from which i am getting SimpleLink library
which we need for this project
but i am keep getting this error from CCS studio named :
unresolved symbols remain
and the error message is :
Building target: "WiFi_transmission.out"
Invoking: Arm Linker
"C:/ti/ccs1120/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=vfplib -me --define=cc3220s -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi -z -m"WiFi_transmission.map" --heap_size=0x0 --stack_size=0x512 -i"C:/ti/ccs1120/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/lib" -i"C:/ti/ccs1120/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="WiFi_transmission_linkInfo.xml" --rom_model -o "WiFi_transmission.out" "./main.obj" "./driverlib/adc.obj" "./driverlib/aes.obj" "./driverlib/can.obj" "./driverlib/comp.obj" "./driverlib/cpu.obj" "./driverlib/crc.obj" "./driverlib/des.obj" "./driverlib/eeprom.obj" "./driverlib/emac.obj" "./driverlib/epi.obj" "./driverlib/epi_workaround_ccs.obj" "./driverlib/flash.obj" "./driverlib/fpu.obj" "./driverlib/gpio.obj" "./driverlib/hibernate.obj" "./driverlib/i2c.obj" "./driverlib/interrupt.obj" "./driverlib/lcd.obj" "./driverlib/mpu.obj" "./driverlib/onewire.obj" "./driverlib/pwm.obj" "./driverlib/qei.obj" "./driverlib/shamd5.obj" "./driverlib/ssi.obj" "./driverlib/sw_crc.obj" "./driverlib/sysctl.obj" "./driverlib/sysexc.obj" "./driverlib/systick.obj" "./driverlib/timer.obj" "./driverlib/uart.obj" "./driverlib/udma.obj" "./driverlib/usb.obj" "./driverlib/watchdog.obj" "../cc3235sf.cmd" -llibc.a
<Linking>
warning #10247-D: creating output section "vtable" without a SECTIONS specification
warning #10443-D: The ".stack" section size is required to be aligned to 8 bytes, but the specified size, 0x512, is not. The aligned size is 0x518
undefined first referenced
symbol in file
--------- ----------------
CPUbasepriGet ./driverlib/interrupt.obj
CPUbasepriSet ./driverlib/interrupt.obj
CPUcpsid ./driverlib/interrupt.obj
CPUcpsie ./driverlib/interrupt.obj
CPUwfi ./driverlib/sysctl.obj
SysCtlDelay ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "wifi_proj.out" not built
plz can someone who has worked on it can reply how to solve this error