Other Parts Discussed in Thread: CC2650, CC2640, CC3120
We have a product where we have 3 TI devices, a MSP432 as the main controller a CC2650 for Bluetooth and a CC3130 for WiFi. The MSP communicates with the two other devices using a 'Simplelink' layer and all works well. We have recently noticed that some of the products exhibit a reset issue where they work for various periods e.g. 45s, 75s, 190s and then reset. It seems to be that the communication with the CC3130 is getting stuck in that there is no response back to the MSP and the watchdog then causes the reset.
Is this a known issue and is there a resolution for it, if not has this been seen before and is there a solution that I can implement.