Part Number: CC3230SF
Other Parts Discussed in Thread: CC3230S, UNIFLASH
Tool/software:
Hi,
My customer has developed their own board with CC3230SF12RGKR.
They want to write software via XDS110, but can’t do that now. They’re not sure if it can be connected correctly to CC3230.
When XDS is connected to PC, “NOserial” is displayed. Is the XDS110 connected correctly ?

They want to confirm the JTAG connection.
There is the following description in the XDS Debug Probe User's Guide.
2.3 Debug Interface
The XDS110 probe supports a debug connection interface through the standard CTI-20 connector (see Section 2.3.1). The supported debug features include:
- 5-pin 1149.1 JTAG connection (including TRSTn)
Does this 5-pin mean Pin 1, 2, 3, 7 and 11 of CTI-20 ?
Is the connection below correct ?
「CTI-20」 - 「CC3230S」
TMS - Pin20
TCK - Pin19
TDO - Pin17
TDI - Pin16
RESET - Pin32
TX and RX of UART are input? or output? from UART point of view.
「XDS110」 - 「CC3230S」
UARTRX - Pin57
UARTTX - Pin55
Thanks and regards,
Hideaki