Part Number: LAUNCHCC3220MODASF
Tool/software:
Hello Ti tech team,
I am currently working with the cc3220modasf and attempting to integrate the local OTA (simplelink_cc32xx_sdk_4_10_00_07) sample code into the Iothub_client_sample_mqtt code (azure_cc32xx_4_10_01_01) by performing the following operations.
1. Include Files
- `ota_archive.c`
- `ota_archive.h`
- `ota_json.c`
- `ota_json.h`
2. Linking Library
- `ti/utils/json/lib/ccs/m4/json_release.a`
I am experiencing the following linking errors.
undefined first referenced
symbol in file
--------- ----------------
CryptoCC32XX_config C:/ti/simplelink_cc32xx_sdk_4_10_00_07/source/ti/drivers/lib/drivers_cc32xx.aem4<CryptoCC32XX.oem4>
CryptoCC32XX_count C:/ti/simplelink_cc32xx_sdk_4_10_00_07/source/ti/drivers/lib/drivers_cc32xx.aem4<CryptoCC32XX.oem4>
The properties of my project are detailed below.
which library path include, or which header file include to fix this problem?