Hi there, I am new to the forum and new to the CC3100.
I discovered CC3100 through TI's website and especially the following caught my attention:
- CC3100 - A Wireless Network Processor with on-chip Wi-Fi, internet, and robust security protocols. It can be used to connect any low-cost, low-power microcontroller (MCU) to the Internet of Things (IoT)!
Seeing that I have a Launchpad and a few MSP430G2553's, I want to create a super simple temperature monitor or so, and then push the data to the CC3100 via UART or I2C or some other serial communication. I want to keep costs low so the MSP430G2553 powered by a couple of AA batteries with the CC3100 at $20 seems like a very cheap IoT solution.
My understanding was you can program the CC3100 to do a certain thing, and then it will just keep on going being in a e.g. station mode, sending out a UDP packet or even making HTTP requests to a server on the local network.
So I went ahead and bought the CC31000BOOST and the CC31XXEMUBOOST.
I am confused though. I can't find a way to simply load some code onto the CC3100 and then leave it to do its thing - such as receiving input from any other MCU and then running some custom code.
Does it seem like I should have bought the right kit for what I want? Should I have bought the SimpleLink CC3100 Module Boosterpack instead? (i.e. http://www.ti.com/tool/TIDC-CC3100MODBOOST)
Thanks