Other Parts Discussed in Thread: CC3100, TIDC-CC3ANTENNA-SELECTION
Hello,
We are using CC3100 in our project. regarding power input , in the datasheet preregulated input is mention.
but the input is 1.85V. where as with VBAT it is 3.3V.
The question is can we use 3.3V input with external LDO or it is limited to 1.85v. the concern is to avoid using internal dc dc regulator to reduce the heat dissipation of the chip.
Planning to provide option for both internal as well external regulator to compare the thermal characteristics.
Kindly could you share schematics design with external power supply input. in the CC3100 datasheet page 31 has a reference circuit. can this be used as it is, or any change required in the circuit?
regarding the Antenna, AH316M245001-T is used in the reference design. is the design tested with alternate antenna for better performance. Could you advice few parts.
kindly reply ASAP
Regards,
Sumathi