This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: Embedded Programming

Part Number: CC3220

I’m facing a trouble to program the SFLASH via UART by using Embedded Programming.
Referring document is “CC3120 and CC3220 SimpleLink™ Wi-Fi® Embedded Programming” at www.tij.co.jp/.../swpa230.pdf.

I think, from STEP1 to STEP10 are completed correctly, because an acknowledge “Last Status response:0x40” is backed by Get Status Command.
After that, Wi-Fi FW USF file which is created by using Image Creator is programed as STEP11.
However image is not programed properly.

Question1: What’s the format to program the SFLASH?  (UCF?)
Question2: I send the data with the following format at once. Is it correct?
 Packet size:   2byte (4096)
 Checksum:  1byte
 FS Programming command:  1byte(0x34)
 Key size:  2byte (0)
 Chunk size:  2byte (4096)
 Flags : 4byte (0)
 Data :  4084 byte(FW)
Question3: Could you please advise me the points which I confirm to solve it.