Other Parts Discussed in Thread: WL1837
Hi, all
our customer used our module(WL1837), and configued the WL1837's BT as the master
if the PCM-CLK configued to 2MHz(or 1MHz), there is a jitter cr ossing with the PCM_CLK(on calling).
and if configued to 256KHz(or 512KHz),the PCM-CLK is OK.
The issue is the same when we used the TI’S WL1837 EVB(configued to 2048 and set loopback mode )
So if the PCM_CLK of WL1837 chipset can’t support the high frequence (>512KHz) when BT configured to be master?
or there are other reasons?
Expect your reply ,TKS