Other Parts Discussed in Thread: CC2564
Dear TI Engineer,
I am a software engineer from a Chinese company, I have some issues when porting CC2564 HFPAGDemo on a cortex-m mcu like smt32, and the evk is cc2564modnem, I have verified my hardware by a3dpdemo_sink and a3dpdemo_src, so the i2s and uart interfaces is works well, but when I running HFPAGDemo,the headset links well, and the uart output logs look like the same with which shows on ti-wiki(processors.wiki.ti.com/.../CC256x_TI’s_Bluetooth_Stack_Basic_HFGAGDemo_APP), but I can't heared any sound form headset or CC2564modnem, the logs showed below:
Please give any ideas or suggestions?
SHELL>> bt start
Start BT App... OpenStack().
HCI_VS_InitializeAfterHCIReset
HCI_VS_InitializeAfterHCIReset Success
Bluetooth Stack ID: 1
WBS Support initialized.
Device Chipset: 4.1
BTPS Version : 4.0.2.1
Project Type : 6
FW Version : 7.26
App Name : HFPAGDemo
App Version : 0.1
LOCAL BD_ADDR: 0xCC78AB32F6DE
GAP_Set_Connectability_Mode(cmConnectable).
GAP_Set_Discoverability_Mode(dmGeneralDiscoverable, 0).
GAP_Set_Pairability_Mode(pmPairableMode).
GAP_Register_Remote_Authentication() Success.
******************************************************************
*Command Options: Inquiry, DisplayInquiryList, Pair, *
* EndPairing, PINCodeResponse, PassKeyResponse, *
* UserConfirmationResponse, *
* SetDiscoverabilityMode, SetConnectabilityMode,*
* SetPairabilityMode, * * ChangeSimplePairingParameters, *
* GetLocalAddress, SetLocalName, GetLocalName, *
* SetClassOfDevice, GetClassOfDevice, *
* GetRemoteName, ManageAudio, *
* OpenAudioGatewayClient, CloseAgClient, *
* ServiceDiscovery, UpdateControlIndicators, *
* CallWaiting, SendCallerIdNotification, *
* SetRingIndication, RingIndication, *
* SetVoiceRecognitionActivation, *
* SetSpeakerGain, SetMicroPhoneGain, *
* DisableRemoteSoundEnhancement, *
* SendOperatorInfo, SendIncomingCallState, *
* SendSubNumber, SendCallList, *
* Help *
******************************************************************
HFAGRE16>SHELL>> bt inquiry
BT cmd:inquiry Return Value is 0 GAP_Perform_Inquiry() SUCCESS.
HFAGRE16>SHELL>> GAP Inquiry Entry Result: 0xA000A000B5EA.
HFAGRE16> GAP_Inquiry_Result: 1 Found.
GAP Inquiry Result: 1, 0xA000A000B5EA.
HFAGRE16>bt ServiceDiscovery 1 12
BT cmd:ServiceDiscovery 1 12
SDP_Service_Search_Attribute_Request(Handsfree) Success.
HFAGRE16>SHELL>> SDP Service Search Attribute Response Received (Size = 0x0010)
Service Record: 1:
Attribute ID 0x0000 Type:
Unsigned Int = 0x00010000
Attribute ID 0x0001
Type: Data Element Sequence
Type: UUID_16 = 0x111E
Type: UUID_16 = 0x1203
Attribute ID 0x0004
Type: Data Element Sequence
Type: Data Element Sequence
Type: UUID_16 = 0x0100
Type: Data Element Sequence
Type: UUID_16 = 0x0003
Type: Unsigned Int = 0x02
Attribute ID 0x0005
Type: Data Element Sequence
Type: UUID_16 = 0x1002
Attribute ID 0x0006
Type: Data Element Sequence
Type: Unsigned Int = 0x656E
Type: Unsigned Int = 0x006A
Type: Unsigned Int = 0x0100
Attribute ID 0x0009
Type: Data Element Sequence
Type: Data Element Sequence
Type: UUID_16 = 0x111E
Type: Unsigned Int = 0x0106
Attribute ID 0x0100
Type: Text String = Hands-Free unit
Attribute ID 0x0311
Type: Unsigned Int = 0x001F
HFAGRE16>bt OpenAudioGatewayClient 1 2
BT cmd:OpenAudioGatewayClient 1 2
Bluetooth Device Address: 0xA000A000B5EA
Open Remote HandsFree Port = 0002
HFRE_Open_Remote_HandsFree_Port: Function Successful ID = 0001.
OpenRemoteHandsFreePort: HFRE_Update_Current_Control_Indicator_Status Function Status 0.
HFAGRE16>SHELL>>
atPINCodeRequest: 0xA000A000B5EA
Respond with the command: PINCodeResponse
HFAGRE16>bt PINCodeResponse 0000
BT cmd:PINCodeResponse 0000 PINCodeResponse.
GAP_Authentication_Response(), Pin Code Response Success.
HFAGRE16>SHELL>> atLinkKeyCreation: 0xA000A000B5EA
Link Key: 0x0C276F4DBE47B8FD151C0D99B50AB240
Link Key Stored locally.
HFAGRE16> HFRE Open Port Confirmation, ID: 0x0001, Status: 0x0000.
HFAGRE16> HFRE Open Service Level Connection Indication, ID: 0x0001
RemoteSupportedFeaturesValid: TRUE
RemoteSupportedFeatures: 0x0000001F
RemoteCallHoldMultipartySupport: 0x00000000
HFRE_Enable Call Line Identification
HFAGRE16>HFRE Call Waiting Notification Activation Indication, ID: 0x0001, Enabled: TRUE.
HFAGRE16>HFRE Call Line Identification Notification Activation Indication, ID: 0x0001, Enabled: TRUE.
HFAGRE16> Unknown HFRE Event Received: 11.
HFAGRE16>SHELL>> bt RingIndication
BT cmd:RingIndication HFRE_Ring_Indication: Function Successful.
HFAGRE16>SHELL>> bt SendCallerIdNotification +9198787899889
BT cmd:SendCallerIdNotification +9198787899889
HFRE_Send_Call_Line_Identification_Notification: Function Successful.
HFAGRE16>SHELL>> bt ManageAudio 1
BT cmd:ManageAudio 1
HFRE_Setup_Audio_Connection: Function Successful.
HFAGRE16>SHELL>> HFRE Audio Connection Indication, ID: 0x0001, Status: 0x0000.
HFAGRE16>