I'm using the CC3100MODBOOST board in AP mode attached to another board for development.
After entering AP mode (which I have verified working by connecting with a secondary device,) I stop the DHCP server, set the config, and then attempt to start it.
Both when entering AP mode and when attempting to start the AP mode I get a general event of type SL_DEVICE_FATAL_ERROR_EVENT with Status -83 (SL_ERROR_DHCP_SERVER_ENABLE_FAILED) and sender 11 (SL_ERR_SENDER_DHCP_SERVER).
sl_NetAppStart(SL_NET_APP_DHCP_SERVER_ID) returns with error code -6.
FW and driver versions:
ID(67108864) FW(31.1.5.0.2) PHY(1.0.3.37)
NWP(2.11.0.1) ROM(13107) HostDrv(1.0.1.11)
NWP log attached:
71�� y �� � <�Z`8 \�; *v"