Hi. TI.
Which of TI's wifi modules meet the following conditions?
=============================
1. Only RF Module.
2. non-OS
3. Contention-Free-Service
=============================
Thank you in advance.
Regards,
Simon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi. TI.
Which of TI's wifi modules meet the following conditions?
=============================
1. Only RF Module.
2. non-OS
3. Contention-Free-Service
=============================
Thank you in advance.
Regards,
Simon
Hi Simon,
Any CC32xxMOD or CC31xxMOD module meets that points. But if you want to use module without application processor (capability to run own code inside module), you can use CC31xxMOD devices. All CC32xx/CC31xx devices supports transceiver mode which allow to use IEEE 802.11 PHY as your own connection- less transceiver.
Jan
Hi Simon,
Yes CC31xxMOD devices supports AP mode. CC3100 supports AP mode for one connected client, CC3120/CC3135 supports up to four clients.
No. AP mode (Soft AP) is a connected mode. By natural behaviour/design of any WiFi device is that AP mode cannot be a connection-less service.
Jan
Hi Jan,
This sounds promising, and one more question.
We want to make our own MAC layer protocol, for response time critial Factory Automation application, which has one hunder slave devices with need tiny bits of TX/RX data each.
Basically, we do not want to be limted by 802.11 mac protocol, which has lots of backoff time and number of connection limits.
If we use CC31xxMOD in transceiver mode, can we fully bypass 802.11 MAC protocl, which has backoff time and connection limit?
Regards,
Simon
Hi Simon,
Yes, it is achievable at transceiver mode with CC31xx devices. As I remember one of e2e forum user had developed own mesh network solution with CC3200 devices.
Btw ... Why you want to develop own MAC layer with WiFi PHY? This can be pretty challenging thing. It should be much easier to use wireless SoC (Sub-1GHz or 2.4GHz) with capability for protocols like a Thread, Zigbee, or 6LoWPAN.
Jan
Hi Jan,
Your advice was very helpful.
I want to try the project.
Please help me in configuring the development environment.
================================================================
1. EVB
Which product should I purchase from the following URL?
www.ti.com/.../CC3120MOD
2. SDK
Where can I download the SDK that supports Non-OS?
================================================================
Regards,
Simon
Hi Simon,
This depends on your host processor. To be able use CC3120MOD with non SimpleLink devices (MSP432, some CCxxxx chips) you need to port host driver to your platform. This can be challenging thing and it will require some resources at your main MCU. As resource of information you should use SIMPLELINK-SDK-WIFI-PLUGIN, SWRU455 at chapter 19. Information sources are mainly related to RTOS implementation, but at e2e forum you find some threads related porting host driver to non-RTOS environment.
I think for start you should buy:
But there can be another way. You can use CC3220MOD and prepare your own MAC firmware for them. Communication with your main MCU will be via your own protocol (e.g. UART, SPI) and your MAC stack will run inside Application processor (Cortex-M4). This approach will off-load your main MCU from any MAC stack handling. BOM price will be similar and you porting of host driver to your main MCU will be not required. Disadvantage of this approach is that you will need to program two MCUs (your main MCU and application processor inside CC3220).
Jan
Hi Jan,
I have a question while checking the following URL.
https://www.ti.com/lit/ug/swru455l/swru455l.pdf
It is stated that the CC3120MOD does not support Real time RSSI.
I understood that RSSI information is not included in the received packet information (Radiotap Header).
Is it correct what I understood?
Should STA use another module (ex)CC3130MOD) to check RSSI?
Regards,
Simon