Hi Team,
Posting for our customer. They intend to use CC3220SF in their project. From our understanding of the datasheet, the Serial Flash (NOR) with maximum size of 256KB is required for storing Application code, WIFI credential and so on. But along with this flash they want to use 1GB NAND flash for caching media
Is it possible to use Serial Flash SPI interface for both NOR and NAND ICs in SPI sharing mode using CS? The intention is to run Application code from Internal flash (1MB) which is available in CC3220SF.
Thanks in advance!
Kind Regards,
Jejomar