Part Number: CC3220
I'm running the latest free rtos publish subscribe example from the aws iot plugin and can not get it to work. I get the following output:
Starting the AWS IoT example application
startSNTP: Current time: Sun Nov 18 19:39:57 2018
CC32XX has connected to AP and acquired an IP address.
IP Address: 192.168.0.41
Flashing certificate file ...
Successfully wrote file /cert/ca.pem to flash
Flashing certificate file ...
Successfully wrote file /cert/cert.pem to flash
Flashing certificate file ...
Successfully wrote file /cert/key.pem to flash
AWS IoT SDK Version 3.0.1-
Connecting...
ERROR: runAWSClient L#108
Error(-7) connecting to a2wpu4ebbjacdc-ats.iot.eu-west-2.amazonaws.com:8883
Subscribing...
ERROR: runAWSClient L#126
Error subscribing (-13)
ERROR: runAWSClient L#178
An error occurred in the loop. Error code = -13
Thank you for any help in advance