Hi,
With the lastest sdk, when my cc3235 project is build on linux, it hangs at the first sl_stop.
I have two projects, one with a cc3235modsf and one with a cc3220modasf.
Both can be compiled either on my windows computer or on a raspberrypi in an ubuntu docker container by our continuous integration server.
I have upgraded both products to the latest sdk 3_30_00_04 and service pack (sp_4.4.0.3_3.1.0.5_3.1.0.19 and sp_3.13.0.3_2.0.0.0_2.2.0.6).
Since then the project with the cc3235 gets stuck at the first sl_stop when built on linux. When built on windows it's ok. And the project with the cc3220 is ok on both.
The code is mostly identical between both project.
The issue is present with both ccs9.1/compiler 18.12.2 and ccs9.2/compiler 18.12.3.
With the previous sdk (3_20_01_01) but latest service pack it is ok.
Any idea on what could be the issue?
Do not hesitate to ask for any information!
Best regards,
Cédric