Team,
-Will the WL183x R8.8 SW support included by default in the next Sitara Linux Processor SDK?
or do you always need to manually add it using the instruction provided in the UG SWRU561A?
-The BT stack has been certified against BT 5.1 std. However the UG SWRU561A does not mention anything about BT.
Is the BT side SW that enables 5.1 compliance already included in R8.8? If not what additional SW is needed to enable BT and compliance with BT 5.1?
Is there a new pre-patched ready to use BT 5.1 compatible stack? or should an older stack be used and patched? Then which one and how?
Thanks in advance!
A.