This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 342
Part Number: CC2630
There exists a Z-STACK-ARCHIVE solution for the CC2630 / CC2650 devices supporting the Zigbee HA 1.2.2a Specification. However, this software is not recommended for Zigbee project development due to the following reasons:
Furthermore, these devices cannot support the newer Zigbee profiles such as 3.0 due to flash memory constraints. Therefore no updated software releases will be provided in the future. It is therefore advised that users developing with Zigbee technology do not consider the CC2630 or CC2650 devices as a viable option. TI instead recommends evaluating the SimpleLink™ CC13X2 / CC26X2 platform that includes several advantages such as:
Regards,Ryan
To better aid the community, please click on the "This Resolved my issue" button whenever a post answers your question!
Thanks Ryan,
Good to know!
Regards,
Toby