Other Parts Discussed in Thread: CC1352R
I'm currently trying to use the two kits mentioned in the title to create a Zigbee network with the coordinator (CC1352R1 Launchpad) acting as a thermostat, and the end device (LPSTK SensorTag) acting as a temperature sensor. I bought these two kits to experiment with different features of Zigbee. As I understand it, for these two projects, they require use of the Application UI to commission the two nodes into the same network. In the application notes for the LPSTK it mentions that the CC1352R1 Launchpad acts as the XDS110 for the LPSTK module. When I do this, I am not able to see the consoles for both of the applications. I don't even think the Launchpad is running while it is used as the debugger for the LPSTK. So my question is, how do I successfully commission a Zigbee network using the zc_thermostat and zed_temperaturesensor projects with these two boards/kits?