Other Parts Discussed in Thread: CC2592, CC2530, CC2652P, , Z-STACK
Hi,
we are using a CC2652 as a zigbee coordinator (RC-CC2652PA) with the ZNP original firmware v4.30 (with only PA pins adjustment to work with CC2592 and network key).
There are 19 devices connected, all joined:
- 14 routers with zstack 3.0.2 (CC2530)
- 2 third parties end devices with Zigbee HA
At some point, the coordinator is not able to communicate with some devices and it does not receive any report from them. I've attached the sniffing trace filtered by only the Link Status messages and it is visible the network degradation. In particular, if you filter for coordinator messages, you can see the Link Status List decreasing.
Also, in most of the other routers messages, the coordinator entry disappear.
- What could be the reason of this malfunction? How can we avoid this behavior?
- Why the Link Status messages are not sent periodically?
- Why the device 0x92D7 (always joined) sends only 2 Link Status messages (the second with excellent communication with the coordinator)?
I've attacched the filtered trace for readability, but I can provide the original trace (about 6300 messages) or a part of it.
Thanks for the help,
Antonio