Other Parts Discussed in Thread: Z-STACK
Hi,
I am running the z-stack 3.0 sampleSwitch application in my cc2538 as coordinatoor (ZC) and I can create a mesh network with home automation devices. Until now I only have worked with these kind of devices.
Then, I would like to use smart energy devices to join them to my coordinator. I have a smart energy (SE) device with a install consists of a 64 bit number and a 16 bit CRC (10 bytes). I have read the zigbee smart energy networks allow the installation code to be comprised of either 6-, 8-, 12-, or 16-byte random, hexadecimal number with a 2-byte CRC, however the 3.0 network requires a 16+2 bytes install code.
I have been searching the z-stack for smart energy profile but only find the z-stack 3.0.1 with home automation examples.
Then my question Is it possible to work with SE devices using the z-stack 3.0 and how?
King regards.