Other Parts Discussed in Thread: CC2530, Z-STACK
hi
how can i increase max connected device to coordinator znp or any router device?
should i change something in fw8config ?
in znp and 8051 of cc2530
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
how can i increase max connected device to coordinator znp or any router device?
should i change something in fw8config ?
in znp and 8051 of cc2530
its not allowing me to increase it more than 10 device
when i want to increase it , it give me this error
Error[e16]: Segment XDATA_Z (size: 0x1bd4 align: 0) is too long for segment definition. At least 0x1a5 more bytes needed. The problem occurred while processing the segment placement command "-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were "XDATA:4d1-1eff" Reserved ranges relevant to this placement: XDATA:1-4d0 XSTACK XDATA:4d1-1eff XDATA_Z BIT:0-7 BREG BIT:80-87 SFR_AN BIT:90-97 SFR_AN BIT:a0-af SFR_AN BIT:b8-c7 SFR_AN BIT:f8-ff SFR_AN Error while running Linker
what should i do?
i design my whole project around cc2530 . if it just capable of only 10 or 32 even 60 , i made a mistake to choose it .
what u think i can do to work with it to have more device ? now i cant increase it more than 10
i use zstack 3.0.0
this is my preproccessor
BDB_FINDING_BINDING_CAPABILITY_ENABLED=0 TC_LINKKEY_JOIN NWK_MAX_DEVICE_LIST=10 ZDSECMGR_TC_DEVICE_MAX=30 ZNP_ENABLED FEATURE_SYSTEM_STATS MT_GP_CB_FUNC MT_SYS_FUNC MT_UTIL_FUNC MT_ZDO_FUNC HAL_SPI=FALSE HAL_UART=TRUE NV_RESTORE BDB_REPORTING SECURE=1 TC_LINKKEY_JOIN NV_INIT NV_RESTORE xZTOOL_P1 xMT_TASK xMT_APP_FUNC MT_SYS_FUNC xMT_ZDO_FUNC xMT_ZDO_MGMT xMT_APP_CNF_FUNC xLCD_SUPPORTED=DEBUG MULTICAST_ENABLED=FALSE ZCL_READ ZCL_WRITE ZCL_BASIC ZCL_IDENTIFY ZCL_ON_OFF ZCL_SCENES ZCL_GROUPS xZCL_LEVEL_CTRL POWER_SAVING
can i delete something to have more ram for more device?
im using znp