Part Number: CC2652R
Other Parts Discussed in Thread: Z-STACK, SIMPLELINK-CC13X2-26X2-SDK, SYSCONFIG
Dear TI,
I have created a coordinator based on CC2652 and I used the firmware from the C:\Ti\Zigbee_3_0_Linux_Gateway_1_0_1\Firmware\znp. Initially it was working well later when I tried to add further more devices, the coordinator won't allow to add, the devices count is 12, we are facing a strange problem that the device pairs and removes automatically and this keeps on continuing. What could be the problem, I suspect the end device and tried pairing it with another hub it is pairing well, Please help us to resolve this problem.