This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
I have created a coordinator based on CC2652 and I used the firmware from the C:\Ti\Zigbee_3_0_Linux_Gateway_1_0_1\Firmware\znp. Initially it was working well later when I tried to add further more devices, the coordinator won't allow to add, the devices count is 12, we are facing a strange problem that the device pairs and removes automatically and this keeps on continuing. What could be the problem, I suspect the end device and tried pairing it with another hub it is pairing well, Please help us to resolve this problem.
Hi Karthick,
If I remember correctly then the ZNP firmware included with the ZIGBEE-LINUX-SENSOR-TO-CLOUD demo software uses the SIMPLELINK-CC13X2-26X2-SDK v3.40 which is quite outdated at this point. I recommend you build a new ZNP image using the latest (v5.20) SDK instead. This will fix any Z-Stack bugs which have been resolved in the past year and allow for you to further configure your Zigbee network settings, for example NWK_MAX_DEVICE_LIST (set through SysConfig -> Z-Stack -> Network -> Network Maximum Device List). There are other variables to consider when increasing network size, please refer to SWRA650 and the Z-Stack User's Guide for more information.
Regards,
Ryan
The sniffer log contains several Beacon Requests but nothing else. This is not very useful for further debugging the issue.
Regards,
Ryan
I am facing some problem while taking the trace, btw I need to know how to check the dead nodes in the ZNP, I mean I have added several devices and some devices were not properly removed due to the hardware failure in the end devices, in this situation I feel the device entry is full, in this situation how can I check the device table entries or how to clear the unnecessary entries?
Also is that possible to take backup from one ZNP and restore it to another ZNP?
1. Zigbee 3.0 coordinator and router would age out dead end device automatically after child-aging timeout. You don’t need to take care of it by yourself.
2. You can refer to https://www.ti.com/lit/an/swra671/swra671.pdf to backup and restore ZNP/coordinator
Ok one more question, Is the paired Zigbee end devices work if I flash a new firmware?
As suggested I am trying to update the firmware with latest 5.2 SDK, will the paired devices work without re-adding?
The ZC/ZNP cloning process specifically copies the NV flash memory from the old device to the new one so that network information is retained and can continue without difficulty, thus the devices which have already joined the network do not have to initiate a fresh join procedure as they will be recognized by the cloned ZC/ZNP device. If you are programming new firmware but desire to retain previous device information then make sure the NV memory contents are not overwritten during the firmware update.
Regards,
Ryan
If you flash new firmware, the previous network information would be erased and you have to factory reset your device to join the network from scratch.
Once again, if you retain NV memory then the previous network information will be restored. Otherwise the devices will have to rejoin even with the same Pan ID and channel since the ZC/ZNP no longer has the network key, TC link keys, associated/routing tables, etc. Please provide more specific information regarding cloning tool issues.
Regards,
Ryan
I somehow managed to work with the Cloning tool, but it is not reading with from the tables screenshot attached
It is explained in Section 7 of SWRA671 that MT_SYS_KEY_MANAGEMENT must be pre-defined in order to grant access to security key data.
Regards,
Ryan