Hi Team,
Can you please check and advise with request?
"
I am working on the RF Serial boot loader but it is not working. I followed the configuration that are in the attached document, but it is still not working.
In my setup:
I programmed the RF board with an image with the following configuration and latched “DIO_6” to the ground. Then restart the board to find the backdoor pin is active low so enter into the boot loader and run the SW application “sblAppEx.exe”. But it doesn’t work correctly. The configurations are as follow:
SET_CCFG_BL_CONFIG_BL_LEVEL=0x00
SET_CCFG_BL_CONFIG_BL_ENABLE=0xC5
SET_CCFG_BL_CONFIG_BL_PIN_NUMBER=0x06
SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE=0xC5
"
Thanks in advance
Best Regards
Furkan Sefiloglu