Part Number: CC2652R
Other Parts Discussed in Thread: Z-STACK
I have our own ZED and our own ZR. And I have TI ZR (CC2652 LaunchPad) and TI ZC which is TI Z-Stack Linux Gateway run on x86 PC using CC2652 LaunchPad as znp.
To test our own ZED join via TI ZR to ZC is successfully. To permit join, I can use either by pressing ZR BTN-1 to start commissioning (Case 1) or start permit join from ZC.
To test our own ZED via our own ZR to ZC is failed when I start permit join from our own ZR. (Case 2)
But, to test out own ZED via our own ZR to ZC becomes OK when I start permit join from ZC. (Case 3)
I found Association Permit bit is true for both ZR and ZC in Case 1 & Case 3. But only ZR's Association Permit bit is true for Case 2.
Attachment 20220527_417_ZED_ZR_passed.zip is for Case 1, and 20220527_337_ZED_ZR_failed.zip is for Case 2.
My questions are:
1. To start commissioning step in TI ZR seems set permit join not for itself but for all devices. Where is the source code in SDK example and related spec?
2. For ZED to join, does it need to set the permit join to on for all devices on the path (> ZR > ZR > ... > ZC)? Where is the related spec?
20220527_417_ZED_ZR_passed.zip20220527_337_ZED_ZR_failed.zip
Regards,
Peter.