Part Number: CC2652R7
Other Parts Discussed in Thread: ENERGYTRACE, SYSCONFIG
Tool/software:
sdk: SimpleLink CC13xx CC26xx SDK (6.41.00.17)
ti temperature sensor example: temp_sensor_LP_CC2652R7_tirtos7_ticlang
I tested that when connecting to the openthread network, the current consumed for the first connection (that is, there is no timeout record in the openthread network) is 6~7mA, and the current consumed for other connections is 2~3mA.
What I want to ask is, can this current consumption be reduced?
Thank you



When the current is low, it is in standby mode.