Hi all,
I'm doing some test with CC2530 and the internal 12-bit ADC but the results are very poor..
I use a very high precision Vref of 2500mV in P0_7 and I do a 12bit conversion as in the TI-MAC or Z-Stack hal_adc.c file, but the result are very different from the multimeter measure.
I set the input voltage from 0 to 2500mV and I read the ADC value, but the ADC have a drift from -10mV to 10,15mV after 1995mV from the real value!!
Is possibile to do a software compensation to have a more precise value?
Did anybody have the same problem?
thank you
Regards,
Emanuele