Other Parts Discussed in Thread: Z-STACK, CC2531, CC2538
Hi TI team,
I am excited to test New Z-Stack Linux Gateway with TI Sample Light end device, and successfully control ZED LED when ZED is built with "SECURE=1".
But, when ZED is built with "SECURE=0", then the binding is failed. Moreover, if ZED is built with "SECURE=1" and "SEC_KEY_LEN=128" instead of "SEC_KEY_LEN=16", then the binding is failed.
The behavior I got is the exactly one TI team expect for this new release of Z-Stack Linux Gateway ? Or, there is something wrong I did to cause these two results ?
Thanks.