Hi eveyone !
I'm trying to figure out how to properly use the Zstack linux gateway API, and I hope some of you may be able to help me :)
I got the beaglebone + cc231 dongle and installed everything (flash cc2531, update beaglebone with new debian, deploy zstack on the beaglebone).
Everything works pretty well with the UI (demo application) provided. I managed to add some devices etc.
I'm trying the use the API, via TCP connection, to manage a zigbee network.
As I'm pretty new to using those high level API, I'm did not really find the API documention usefull.
It's okay that packet's payload is preceded by a 4 byte header. The TCP connection is okay (I see my packets pop thru the zigbee servers logs, via SSH) I already have my protobuf serializing lib ready to go, but I did not really find out how the payload packet looks like ?
Is there, somewhere, an example of what a correct packet looks like ? That may seem pretty noobish question, and I guess it is, but I'm stuck with this :)
I hope I'm clear with what I'm looking for. Let me know if you need any information :)