This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sleepy Routers and end devices

Other Parts Discussed in Thread: CC2630, CC2530, CC2538

Hi,


I am struggling with the choise of protocol and devices to use in my application.
I want do design a network where i have 45 sensor nodes that reports their data to an gateway, and this gateway sends the data to the cloud by 3G connection.
I saw that the CC2630 is fine for my end device nodes, but for my gateway I am not sure if it can communicate with the 45 nodes and then send its data to the cloud by 3G (3G module, that communicates by AT commands). In the beginning I decided to use ZigBee for the communication between the nodes and the gateway (star topology), but the more I read, the more confused I get.
The power consumption is very important since all the devices (nodes and gateway) are battery powered. So I will have sleepy routers and sleepy nodes.


Should I use ZigBee or 6LoWPAN?


Can I use CC2630 in end devices and gateway?

Thank you so much.