Greetings all,
I'm going to use my CC2650EMK alone without the SmartRF board. I want to make sure I use the right voltage levels, so I have some questions:
1) Can I use this connection to power the module?
GND: P1-1 (Connector 1 Pin 1)
VDD 3.3V : P2-7 (Connector 2 Pin 7)
2) If I used a GPIO pin as output, does it output logical "1" at 3.3v and logical "0" at GND ?
3) If I used a GPIO pin as input, should I use 3.3v as "1" and GND as "0" ?
Thanks in advance.
Regards,
* James *