This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: IQxel test method?

Part Number: CC2531


Dear TI Experts,

My customer is testing RF parameter of CC2531 with IQxel , they use "packet TX" in SmartRF Studio to control CC2531, however, they can only measure power in IQxel .

they want to measure below paramater. Could you kindly advise how to config SmartRF Studio to measure these parameters? Thanks a lot.

TX:Freq Error、EVM、OffsetEVM、Power、Spectrum Mask

RX:PER、RSSI

Below is the test platform:

IQxel :

SmartRF Studio:

  • Hi Ke Huang,

    Why do they need to test these parameters on the CC2531 USB dongle? They can find them in the datasheet.

    Anyway, what they are asking about is related to IQxel configuration, not the CC2531.

    Regards,
    Fredrik
  • Hi Fredrik K,

    we need to test the parameters in the production at factory ,to avoid parameter deviations due to non-consistency of each incoming  componients.

  • Hi Yaojun,

    Ok, so this is a production test setup, not for evaluation?

    If so I would consider simply running a sequence of sending and receiving packets between the DUT and a CC253x device. This will verify that the DUT actually transmits and receives correctly. Additionally, measuring the current consumption of the DUT during TX and RX can tell you if it works as intended or not (missing components can for example lead to deviations in RF currents). The CC253x devices also have an internal register to read out frequency offset of incoming packets.

    Back to the original question, what you are asking is tied to the setup of the IQxel instrument itself. If the instrument has requirements on data format you have to configure SmartRF Studio accordingly. Note that the current selected option in Studio sends a continuous stream of randomly modulated data, not packets. If packets are required you must change to "Packet TX".

    Regards,
    Fredrik