This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352R: Z-Stack examples licensing for open source project

Part Number: CC1352R
Other Parts Discussed in Thread: Z-STACK

Tool/software: Code Composer Studio

Dear Support,

As part of a research project´s results, I would like to publish a CCS project´s source code on GitHub. The software was developed for our own hardware, which is not for sale but also offered as reference design. The project is however based on Simplelink’s Z-Stack examples, therefore I was wondering if any kind of license is required (i.e. BSD) or a simple MIT License could be used. Do you have any experience on that? I appreciate your help.

Regards,

Angel

  • Hi,

    Have you already seen the manifest in the SDK?
    If not, please see <SDK installation>/manifest_simplelink_cc13x2_26x2_sdk_*.html. It has license information.

    Regards,
    Toby

  • Thanks Toby,

    I understood that the manifest lists the licenses used for every part of the SDK. Do I need to specify this in a license/manifest file as well? or having the copyright header on every source code file as provided by TI is enough?

    Moreover, is the license_xxxxx.txt to be included on my project´s root directory? I appreciate your help on this.

     Best Regards,

    Angel

  • Should be ok if you keep the BSD3 header on all each file and follow what the header instructs.

  • Perfect, thanks for your help.

    Regards,

    Angel