Part Number: CC2538
Other Parts Discussed in Thread: CC2530, Z-STACK
Hi,
I read this thread:
CC2530: Zigbee Broadcast msg for RSSI Location (AF_SKIP_ROUTING)
e2e.ti.com/.../cc2530-zigbee-broadcast-msg-for-rssi-location-af_skip_routing
I understand the problem. The end device is always routing via its parent and hence a broadcast is actually a relayed broadcast. However, mention was made of ZDP_DeviceAnnce. In fact, this works, I tested with 1 coordinator and 2 routers, an end device announce is received by both routers. So my question is, how do you extract the LQI & RSSI of this announce ? It seems that the structures for zdoIncoming message doesn't have these, but afIncomingMSGPacket_t does ? I am using ZStack 3.0.2 and GenericApp to test. Are these values captured by the stack in this instance ? If they are, how do you extract them ?
typedef struct
{
osal_event_hdr_t hdr;
zAddrType_t srcAddr;
uint8 wasBroadcast;
cId_t clusterID;
uint8 SecurityUse;
uint8 TransSeq;
uint8 asduLen;
uint16 macDestAddr;
uint8 *asdu;
uint16 macSrcAddr;
} zdoIncomingMsg_t;
typedef struct
{
osal_event_hdr_t hdr; /* OSAL Message header */
uint16 groupId; /* Message's group ID - 0 if not set */
uint16 clusterId; /* Message's cluster ID */
afAddrType_t srcAddr; /* Source Address, if endpoint is STUBAPS_INTER_PAN_EP,
it's an InterPAN message */
uint16 macDestAddr; /* MAC header destination short address */
uint8 endPoint; /* destination endpoint */
uint8 wasBroadcast; /* TRUE if network destination was a broadcast address */
uint8 LinkQuality; /* The link quality of the received data frame */
uint8 correlation; /* The raw correlation value of the received data frame */
int8 rssi; /* The received RF power in units dBm */
uint8 SecurityUse; /* deprecated */
uint32 timestamp; /* receipt timestamp from MAC */
uint8 nwkSeqNum; /* network header frame sequence number */
afMSGCommandFormat_t cmd; /* Application Data */
uint16 macSrcAddr; /* MAC header source short address */
uint8 radius;
} afIncomingMSGPacket_t;
Regards,
Ian