This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: Antenna Switch protection (TVS diode)

Part Number: CC2652P
Other Parts Discussed in Thread: CC1352P, TPD1E04U04

Hello,

We have our design with CC2652P based on the CC1352P LAUNCHPAD-2. In the antenna switch you have this TVS diode (swrc350a reference design): 

Unfortunately, this TPD1E0B04DPY is out of stock. We are thinking about using TPD1E1B04DPYT instead. The main differences are clamping voltage of 8.5V instead of 19V, and IO Capacitance of 1pF instead of 0.18pF. Do you think this will affect the performance of the antenna? In that case, do you have any other TVS diode to recommend to us, or it would just be better to not use it at all?

Thanks!