Other Parts Discussed in Thread: BLE-STACK
Hi all, I need to advise about GATT profile topology. I need to implement special primary service which can be register for multiple times with the same UUID. I try implement this concept with SimpleBLEPeripheral sample code in ble-stack library. I do this by calling GATTServApp_RegisterService function for two times with the same parameters. When I read GATT profile from client-side only one service with this UUID was published. Could anybody advise me if it is correct behavior or is it bug? I found no information about this case. GATT_DiscPrimaryServiceByUUID function has notice in description (TI_BLE_Vendor_Specific_HCI_guide document) that "The specific primary service may exist multiple times on a server", so I would expect that it is possible that profile may contains primary services with the same UUID. Thank for any advice, Martin Petrik