Setting the PENDING_OR in FRMCTRL1 seems to override any manual setting made using the SACK and SACKPEND strobes, i.e. issuing SACK has the same result as SACKPEND when PENDING_OR = 1.
Is there a way to avoid this behavior other than clearing the PENDING_OR flag prior to issuing the SACK command?
Since this is in a timing-critical path, I would like to avoid an unnecessary SPI transfer.
Is there a way to have the pending bit = 0 in the ACK frame, if the ACKed frame is not a MAC data poll command using hardware features of CC2520?
Thanks
Arasch