Hi,
I'm trying to configure the CC3100.
I tried calling sl_WlanPolicySet(...) before calling sl_Start(), but the process gets stuck within the simplelink code.
I understand that nothing can be done before calling sl_Start(). Even sl_Stop() gets stuck - is this assumption correct?
Looking at the TI examples (getting_started_with_wlan_ap), I can be calling sl_Start() 3 times till the CC3100 is configured as needed:
1 - Establish connection.
2 - Change to AP (if in STA)
3 - restart the CC3100 after configuration
Is there a way to quicken things? Can I make AP configuration changes even if the CC3100 is in STA, thus merging 2 and 3?