I've been testing the RF430CL330H in an unpowered configuration. With just the RF430CL330H EVM and no MCU attached, I cannot read and write it. With an MCU attached (also unpowered, and with VCC connected to RF430CL330H) I can read and write it.
Does the RF430CL330H require configuration by an MCU before it can allow reading or writing from an external NFC device? If so, what exactly has to be set up? Is it just the RF enable, or are there other registers that need to be set?
Is a reset of the RF430CL330H required? Using the example code from sloc303, it doesn't work if I remove the reset.
While the unpowered operation seems to work using just EVMs, I’m concerned with how this will work in a larger system. The RF430CL330H is waking up and suppling VCC to the MCU, which allows it to wake up and run. But if this VCC rail is connected to other components, the RF430CL330H will not be able to supply enough power to the rest of the system, and the R/W will not work. Do we need to isolate the power to the MCU+NFC so that only that part of the circuit powers up?