I am following the out of box demo step by step and I have run into a road block In the steps it says to download the TI sensor AP for IOS and I have and it works as instructed until step 3 of the section on downloading images OAD. In item 2 &3 it instructs to make one device a concentrator by downloading from the list on the phone the Concentrator firmware for the US version. Although the file named in the text does not exist there is a file for this version which is 1.45 with 1.33 firmware. The next step instructs to download the Node firmware from the same location. However, it does not exist there are node files for EU but none for the US.
There is another phone AP by TI called the SimpleLink starter, this is very confusing because it is not mentioned anywhere but in its firmware update files a file to create a 1350 tag node does exist but it is for version 1.51 so it instructs to update the firmware in version 1.45. However, there is a version A and B and I am not sure which one to use or if it is for the 1350 sensor tag.
Could anyone sort this out for me/ Thank you